We are using this processor in an embedded radar system and are trying to program it so that we can download a new program via the internet and then execute the new code once it has been stored in memory. This way we can support our products in the field with software updates as necessary.
We are able to download the program and store it in memory. However, when we try to boot from this new program, the processor stops during the initialization phase of the program and then exists.
Is there anyone available that we can talk to that has done this type of programming (we are using C) or maybe do a Webex to help find our problem? If yes, can you please provide a name and contact information? Any help on this topic would be greatly appreciated.
Sincerely,
Bob Onesti