Hi,
I have read some posts related with the VPBE Digital LCD Timing, but I am still confused about it, so i need some help.
In VPBE user guide, it said that the unit is the enc clock that is VENC clock.
In my DM6446 board, VENC clock is set to 27MHZ and DCLK for my LCD panel is 6.75MHZ and the LCD resolution is
240x320. So if the user guide is right, the value of HVALID should be 4*240, not 240. Is there anyone here could tell
me the right answer of HVALID value?
I will be appreciated for any help,
Thank you,
htbegin