Have you been able to resolve this? I have perfectly the same problem.
Downloaded the Demo Code ADS1298 ECG MDK under C5515 EVM from http://code.google.com/p/c5505-ezdsp/.
Did the change in C/C++ Build Include Options following the instructuin posed in this Forums so that the code can be successfully built.
However, there are still problems:
1. Changed the code according to the ReleaseNote to enable the LCD on the EVM5515, but there are only words "ECG MONITOR; II BPM" and no waveform.
2. The PC Application always shows "Serial Port Disconnected" and no ECG waveform observed. Don't know the installation of the PC Application is corrected.
Any tips?
Thanks