Hi,
I have a question about C5517 TRM description.
In C5517 TRM(SPRUH16B) page.141 "1.7.5.2 Peripheral Reset Control Register(PRCR)",
it seem that there are typo in Figure 1-61.
In Figure 1-61, it said that bit[6] McBSP_RST of PRCR register is "Read-only".
Is this means that McBSP can not be reset by writing 1 to PRCR bit[6]?
Or is it just a typo, and bit[6] McBSP_RST is Read and Write bit field?
best regards,
g.f.