Other Parts Discussed in Thread: TMS320DM6467
hi,
i am working on dm6467EVM and my vision is "to port android kernel on to the board and then able to encode & decode the audio, video streams"
For that 1)i ported android kernel 2.6.35 on the tms320dm6467 and the board is up through nfs mout root file sysem
2)i installed my development host system with android sdk and generated .apk file for playing an audio & vedio application
The both audio & video applications are working fine on emulator(2.6.27 kernel)but when i connected my board and after installation my .apk file through adb (or) through eclipse i am getting following errors from eclipse before to launch my activity
Failed to upload mediaplayer.apk on device '192.168.1.130:5555'
java.io.IOException: Unable to upload file: timeout
Launch canceled!
so, please can any one solve my problem or can suggest a way to develope my project.... and is the work done by me till now is syncing with my project or iam going in wrong way.... will be a great help for me
Thanks
Vijay