Part Number: OMAP-L138
Tool/software: Linux
Hi
I want to use mcbsp interrupt in the linux for omap.I set the mcbsp registers and it seems ok.
I did not found any example for such implementation? Does omap-l138 davinci bsp support it?
regards
Yehuda
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: OMAP-L138
Tool/software: Linux
Hi
I want to use mcbsp interrupt in the linux for omap.I set the mcbsp registers and it seems ok.
I did not found any example for such implementation? Does omap-l138 davinci bsp support it?
regards
Yehuda
Hi
Thnks for the response.
The sdk used is : ti-sdk-omapl138-lcdk-01.00.00
linux omap version is : 3.1.10-gf6fe6d8-dirty.
I want to update the post that I need mcbsp work with EDMA3 and interrupt driven from the EDMA completion event.
I found a link regards OMAP-L1 Linux Drivers Usage which describe mcbsp test kernel object on EVM.
Is it suitable for omap-l138 and I can base on it?
Is it enough?
Is it at DVSDK 4.xx ?
Best Regards
Yehuda