This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5716: McSPI Slave mode

Part Number: AM5716

Hi,

I would like to understand if it is possible to configure the SPI controller of AM5716 as Slave and use it as a Flash Memory. In that case, the SPI master sees the slave device only as a SPI flash memory and performs read accesses only by issuing a read command followed by (say 24-bit) memory address as done in SPI Flash. 

If it is possible, could you please also tell us whether there is a software support to implement this feature in the PSDK?

Regards,

Shareef