Part Number: ADS1220
Tool/software: Linux
Hello,
How can I setup mux to read the value from four independend single ended chanels and how to catch the value? In all examples available on the web I can only see how can I read build-in sensor or read the AVDD voltage. I am sending a command to start sync (0x08) and run the loop to read the value if irq is != 0. In loop I sent 0x10 and read 3 bytes to convert the finall value. What I need to do to read 4 channels? How the values will be send by device?
Best Regards
--