Tool/software: Linux
Hi,
I tried to enable SPI 0 & SPI 4 in AM437X MYD-C437X development board.
I modified .DTS files to Enable SPI0 & SPI4.
spi0_pins: pinmux_spi0_pins {
pinctrl-single,pins = <
0x150 (PIN_OUTPUT | MUX_MODE0 | INPUT_EN)
0x154 (PIN_OUTPUT | MUX_MODE0)
0x158 (PIN_INPUT | MUX_MODE0)
0x15c (PIN_OUTPUT | MUX_MODE0)
>;
};
&spi0 {
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&spi0_pins>;
spidev@0 {
spi-max-frequency = <24000000>;
reg = <0>;
compatible = "rohm,dh2228fv";
};
};
sameway i did for SPI4. But i cant able to see any device under "dev" like /dev/spidev1.0 & /dev/spidev2.0.
ALso, i enable McSPI driver & USER space driver support in kernel.
Please i need support from anyone.