Part Number: PROCESSOR-SDK-AM335X
Other Parts Discussed in Thread: AM3352
Tool/software: Starterware
Hi,
When I load u-boot-spl.bin through UART to my customized am3352 board, I got stuck.
I use am335x-evm.dts with some modification, e.g. remove all mmc info and some other device definition. Sysboot pins are set in order to boot from 'spi, uart, ethernet'. Built with sdk3.3.0.4. Loading u-boot-spl.bin to starter kit through UART, and it prints the compiling information of this SPL and print another C. After this, I can load my u-boot.img.
But when I loaded the same SPL to am3352, file is transferred ok, but there is no more printing. It just stuck there. If I tried to send u-boot.img anyway, I got "timeout on pathname".
I don't have JTAG, and have no idea what is happening. There are no actions on spi or ethernet.
Can anyone give me a hint, what could be wrong?
Thank you.