This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/OMAP-L138: GateMP in multithread app

Part Number: OMAP-L138

Tool/software: Linux

Hi,

I'm using GateMP in my app between single DSP- process and single Linux- process with multiple threads. Gone well so far but when I added one thread more, GateMP- protected area could not be acessed in that thread for some reason.

Should one thread create GateMP and each Linux thread open it or can one global gate handle be used in Linux process?

Tools I'm used can be seen below.

BR, risto

LINUXKERNEL = $(DEPOT)/ti/mcsdk_1_01_00_02/board-support/linux-3.3-psp03.22.00.06.sdk
CGT_ARM_INSTALL_DIR = $(DEPOT)/arago-2011.09/armv5te
CGT_ARM_PREFIX = $(CGT_ARM_INSTALL_DIR)/bin/arm-arago-linux-gnueabi-
IPC_INSTALL_DIR = $(DEPOT)/ti/ipc_1_25_03_15
BIOS_INSTALL_DIR = $(DEPOT)/ti/bios_6_34_03_19
XDC_INSTALL_DIR = $(DEPOT)/ti/xdctools_3_24_05_48