This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Starterware/TDA3: DPLL setting with 27MHz input for SYS_CLK1

Part Number: TDA3

Tool/software: Starterware

Hi experts,

 

I have a query about SYS_CLK1 on TDA3x.

ON TDA3x EVM, 20 MHz crystal is mounted for SYS_CLK1 input.

 If we want to replace it with 27 MHz, we need to change sysboot[9:8] setting from 0b01 to 0b10.

 

In addition to this, we also need to change all 5 DPLL configuration so that each blocks get appropriate frequency of input clocks.

I would like to achieve this with minimum effort.

The idea is to modify only N, M in DPLL_xxx to get the same frequency for CLKOUT.

 

Could you please review if below M, N settings are fine or not?

Original setting (SYS_CLK1: 20 MHz)

  DPLL_CORE DPLL_PER DPLL_EVE_VID_DSP DPLL_GMAC_DSP DPLL_DDR
Ref Clock (MHz) 20 20 20 20 20
N 4 4 7 4 4
M 266 192 238 250 266
CLKOUT (MHz) 1064 768 595 1000 1064

New setting (SYS_CLK1: 27 MHz)

  DPLL_CORE DPLL_PER DPLL_EVE_VID_DSP DPLL_GMAC_DSP DPLL_DDR
Ref Clock (MHz) 27 27 27 27 27
N 26 26 26 26 26
M 1064 768 595 1000 1064
CLKOUT (MHz) 1064 768 595 1000 1064

Thanks & Regards,

-Shibata