This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM5718: PCIe EP question

Part Number: AM5718


Tool/software: Linux

Hello TI Expert,

 

I have got a question from the customer who is evaluating AM5718IDK PCIe with Windows PC.

Would you please check the question?

This is a related with the question below;

e2e.ti.com/.../628862

 

They tried to connect the AM5718IDK (PCIe EP) with Windows PC (PCIe RC).

However, it looks that AM5718IDK cannot be recognized as an EP from the Windows PC.

They powered on AM5718IDK first, then they powered on the Windows PC. But it is not recognized from PC.

 

 

[Question]

If the AM5718 is configured as EP, is any start-up sequence between RC and EP prepared in the AM57x PCIe driver?

We would like to know whether there is a signal like a USB enumeration or not.

We just would like to isolate which side has a problem , Windows or AM57x Linux driver.

Best Regards,

Nobu Arai