Hi,
We are working on a new board with a TMS320DM6467 and a TVP5158.
In the TMS320DM6467datasheet, it is written that the VPIF accept ITU BT.656 (clock at 27 MHz), ITU BT.1120 (clock at 74.25 MHz), SMPTE 296M (clock at 74.25 MHz) and raw data (clock at 99 MHz max) in input.
Firstly, what is the difference between ITU BT.1120 and SMPTE 296M modes ?
Secondly, in the TVP5158 datasheet (page 82), there are application examples which show two connections for D1 applications. The first one show a connection to DM6467 on 8bit@108 MHz and a second one wich is 16bit@54MHz. According to the TVP5158 datasheet (page 25), the 8bit@108MHz is a BT.656 mode and the 16bit@54MHz is a BT.601 mode, but the clock does not match for BT.656 and DM6467 is known to not support BT.601.
Someone could explain it to me ?
Best,
Guillaume