This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: IDK DDR3 data signal connections

Part Number: AM5728

I want to design  one board use the chip AM5728, I find the dd3 data signals are connected in  the schematic of The ARM MPU AM572XX industrial EVM  as follow:

whyit is connected like this: DDR_D0<--->DQ0  DDR_D1<-->DQ1  DDR2<-->DQ2  DDR3<-->DQ3,and so on? the signals  DDR_D0,DDR_D1,DDR_D2,DDR_D3 in the above picture  are the chip AM57XX data signals, and the the DQ0,DQ1,DQ2,DQ3 are the chip ddr3 data signals.if I connet these signals like this:DDR_D0<--->DQ0  DDR_D1<-->DQ1  DDR2<-->DQ2  DDR3<-->DQ3,did I need to modify the driver of ddr3 of the sdk or should I connect these  signals as the evm schematic?