I tried to test decode in dvsdk_3_01_00_10, it failed. But it works with dvsdk_3_01_00_06. Here is log with CE_DEBUG=3. cs.x64P is in the same dir as application.
@5,645,691us: [+7 T:0x40ba5490 S:0x40ba4d64] OP - Processor_create_d> Loading and starting DSP server 'cs.x64P' FAILED, status=[0x80008008] (look for error code 'DSP_EBASE + 0x8' in dsplink*/package
@5,645,752us: [+0 T:0x40ba5490 S:0x40ba4d4c] OP - Processor_delete_d> Enter (proc=0x6e840)
@5,645,813us: [+2 T:0x40ba5490 S:0x40ba4d4c] OP - Processor_delete_d> Closing remote transport...
@5,645,843us: [+6 T:0x40ba5490 S:0x40ba4d4c] OP - Processor_delete_d> Closing remote transport FAILED, status=0x80008002.
@5,645,904us: [+2 T:0x40ba5490 S:0x40ba4d4c] OP - Processor_delete_d> Stopping DSP...
@5,645,935us: [+6 T:0x40ba5490 S:0x40ba4d4c] OP - Processor_delete_d> Stopping DSP FAILED, status=0x80008002
@5,645,996us: [+2 T:0x40ba5490 S:0x40ba4d4c] OP - Processor_delete_d> Closing pool...
@5,646,026us: [+6 T:0x40ba5490 S:0x40ba4d4c] OP - Processor_delete_d> Closing pool FAILED, status=0x80008000
@5,646,087us: [+2 T:0x40ba5490 S:0x40ba4d4c] OP - Processor_delete_d> Detaching from DSP...
@5,646,118us: [+6 T:0x40ba5490 S:0x40ba4d4c] OP - Processor_delete_d> Detaching from DSP FAILED, status=0x80008000
@5,646,149us: [+2 T:0x40ba5490 S:0x40ba4d4c] OP - Processor_delete_d> Destroying DSP... (object, that is)
@5,646,210us: [+6 T:0x40ba5490 S:0x40ba4d4c] OP - Processor_delete_d> Destroying DSP FAILED, status=0x80008000