Part Number: AM3354
Tool/software: Starterware
Dear,
Now I'm trying to use the PDK RTOS 4.00.00.04/pdk 1.0.7 on AM3354 platform.
When doing the UART porting, there are various issues:
The first questions is the UART LLD usage: is it a must to use the UART LLD functions?
What's the differences between the project under the fold of "C:\ti\pdk_am335x_1_0_7\packages\MyExampleProjects" and "C:\ti\pdk_am335x_1_0_7\packages\ti\starterware\examples".
As it is the first time i use this, I need to port the UART driver in a short while, which one is the better choice for me?