Part Number: PROCESSOR-SDK-AM335X
Tool/software: Linux
Hello
No rule to make target 'arch/arm/boot/dts/am335x-icev2-pru-excl-uio.dtb'
I keep getting the above error trying to build for the AM335x starter kit. I am building with:
> bitbake arago-base-tisdk-image
I have added the default MACHINE to the config file and am following the instructions from -processors.wiki.ti.com/.../Processor_SDK_Building_The_SDK
using the pre-downloaded snapshot of the sources from -"software-dl.ti.com/.../am335x-evm-linux-sdk-arago-src-04.00.00.04.tar.xz".
The output I get is:
Loading cache: 100% |#########################################################################| Time: 0:00:04
Loaded 3236 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies
Build Configuration:
BB_VERSION = "1.32.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "Ubuntu-16.04"
TARGET_SYS = "arm-linux-gnueabi"
MACHINE = "am335x-evm"
DISTRO = "arago"
DISTRO_VERSION = "2017.05"
TUNE_FEATURES = "arm armv7a vfp thumb neon callconvention-hard"
TARGET_FPU = "hard"
meta-processor-sdk = "HEAD:3d2f620a6a98b1b6abb1103d7dc986921436ed19"
meta-arago-distro
meta-arago-extras = "HEAD:b727bf8fce8e9cb5a6b5d5b48c45f0088e67eb53"
meta-browser = "HEAD:880a7bd1d3b9a1b2003f5b0620350f03158bbd43"
meta-qt5 = "HEAD:3601fd2c5306ac6d5d0d536e0be8cbb90da9b4c1"
meta-networking
meta-ruby
meta-python
meta-oe
meta-gnome = "HEAD:fe5c83312de11e80b85680ef237f8acb04b4b26e"
meta-ti = "HEAD:41d6fdc0fe5ea6054616cfccda13baac3ff33791"
meta-linaro-toolchain
meta-optee = "HEAD:d84874bad834657dd04ea69c35a74dd9dbd535b8"
meta = "HEAD:ddf907ca95a19f54785079b4396935273b3747f6"
Initialising tasks: 100% |####################################################################| Time: 0:00:18
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
ERROR: linux-ti-staging-4.9.28+gitAUTOINC+eed43d1050-r22c.arago5.tisdk3 do_compile: oe_runmake failed
ERROR: linux-ti-staging-4.9.28+gitAUTOINC+eed43d1050-r22c.arago5.tisdk3 do_compile: Function failed: do_compile (log file is located at /home/jeff/oe-dir/tisdk/build/arago-tmp-external-linaro-toolchain/work/am335x_evm-linux-gnueabi/linux-ti-staging/4.9.28+gitAUTOINC+eed43d1050-r22c.arago5.tisdk3/temp/log.do_compile.11851)
ERROR: Logfile of failure stored in: /home/jeff/oe-dir/tisdk/build/arago-tmp-external-linaro-toolchain/work/am335x_evm-linux-gnueabi/linux-ti-staging/4.9.28+gitAUTOINC+eed43d1050-r22c.arago5.tisdk3/temp/log.do_compile.11851
Log data follows:
| DEBUG: Executing shell function do_compile
| NOTE: make -j 2 HOSTCC=gcc HOSTCPP=gcc -E zImage CC=arm-linux-gnueabihf-gcc -mno-thumb-interwork -marm -fuse-ld=bfd LD=arm-linux-gnueabihf-ld.bfd LOADADDR=0x80008000
| NOTE: make -j 2 HOSTCC=gcc HOSTCPP=gcc -E am335x-evm.dtb
| NOTE: make -j 2 HOSTCC=gcc HOSTCPP=gcc -E am335x-evmsk.dtb
| NOTE: make -j 2 HOSTCC=gcc HOSTCPP=gcc -E am335x-bone.dtb
| NOTE: make -j 2 HOSTCC=gcc HOSTCPP=gcc -E am335x-boneblack.dtb
| NOTE: make -j 2 HOSTCC=gcc HOSTCPP=gcc -E am335x-bonegreen.dtb
| NOTE: make -j 2 HOSTCC=gcc HOSTCPP=gcc -E am335x-icev2.dtb
| NOTE: make -j 2 HOSTCC=gcc HOSTCPP=gcc -E am335x-icev2-pru-excl-uio.dtb
| ERROR: oe_runmake failed
| CHK include/config/kernel.release
| GEN ./Makefile
| CHK include/generated/uapi/linux/version.h
| CHK include/generated/utsrelease.h
| Using /home/jeff/oe-dir/tisdk/build/arago-tmp-external-linaro-toolchain/work-shared/am335x-evm/kernel-source as source for kernel
| CC scripts/mod/empty.o
| CC scripts/mod/devicetable-offsets.s
| MKELF scripts/mod/elfconfig.h
| HOSTCC scripts/mod/modpost.o
| HOSTCC scripts/mod/sumversion.o
| GEN scripts/mod/devicetable-offsets.h
| HOSTCC scripts/mod/file2alias.o
| HOSTLD scripts/mod/modpost
| CHK include/generated/timeconst.h
| CHK include/generated/bounds.h
| CHK include/generated/asm-offsets.h
| CALL /home/jeff/oe-dir/tisdk/build/arago-tmp-external-linaro-toolchain/work-shared/am335x-evm/kernel-source/scripts/checksyscalls.sh
| CHK include/generated/compile.h
| CHK kernel/config_data.h
| DTC drivers/gpu/drm/tilcdc/tilcdc_slave_compat.dtb
| DTB drivers/gpu/drm/tilcdc/tilcdc_slave_compat.dtb.S
| AS drivers/gpu/drm/tilcdc/tilcdc_slave_compat.dtb.o
| LD drivers/gpu/drm/tilcdc/built-in.o
| rm drivers/gpu/drm/tilcdc/tilcdc_slave_compat.dtb.S drivers/gpu/drm/tilcdc/tilcdc_slave_compat.dtb
| LD drivers/gpu/drm/built-in.o
| LD drivers/gpu/built-in.o
| LD drivers/built-in.o
| LD vmlinux.o
| MODPOST vmlinux.o
| GEN .version
| CHK include/generated/compile.h
| UPD include/generated/compile.h
| CC init/version.o
| LD init/built-in.o
| KSYM .tmp_kallsyms1.o
| KSYM .tmp_kallsyms2.o
| LD vmlinux
| SORTEX vmlinux
| SYSMAP System.map
| OBJCOPY arch/arm/boot/Image
| Kernel: arch/arm/boot/Image is ready
| LZMA arch/arm/boot/compressed/piggy_data
| AS arch/arm/boot/compressed/piggy.o
| LD arch/arm/boot/compressed/vmlinux
| OBJCOPY arch/arm/boot/zImage
| Kernel: arch/arm/boot/zImage is ready
| CC scripts/mod/devicetable-offsets.s
| CC scripts/mod/empty.o
| MKELF scripts/mod/elfconfig.h
| HOSTCC scripts/mod/modpost.o
| GEN scripts/mod/devicetable-offsets.h
| HOSTCC scripts/mod/sumversion.o
| HOSTCC scripts/mod/file2alias.o
| HOSTLD scripts/mod/modpost
| make[3]: *** No rule to make target 'arch/arm/boot/dts/am335x-icev2-pru-excl-uio.dtb'. Stop.
| arch/arm/Makefile:336: recipe for target 'am335x-icev2-pru-excl-uio.dtb' failed
| make[2]: *** [am335x-icev2-pru-excl-uio.dtb] Error 2
| Makefile:150: recipe for target 'sub-make' failed
| make[1]: *** [sub-make] Error 2
| Makefile:24: recipe for target '__sub-make' failed
| make: *** [__sub-make] Error 2
| ERROR: Function failed: do_compile (log file is located at /home/jeff/oe-dir/tisdk/build/arago-tmp-external-linaro-toolchain/work/am335x_evm-linux-gnueabi/linux-ti-staging/4.9.28+gitAUTOINC+eed43d1050-r22c.arago5.tisdk3/temp/log.do_compile.11851)
ERROR: Task (/home/jeff/oe-dir/tisdk/sources/meta-ti/recipes-kernel/linux/linux-ti-staging_4.9.bb:do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 1077 tasks of which 1069 didn't need to be rerun and 1 failed.
Summary: 1 task failed:
/home/jeff/oe-dir/tisdk/sources/meta-ti/recipes-kernel/linux/linux-ti-staging_4.9.bb:do_compile
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.