This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/TMDXSK437X: EVM issues

Part Number: TMDXSK437X


Tool/software: Linux

How to launch a terminal console and configure the IP of ethernet interface ?

I´m using TMDXSK437X, it cames with a SD card that has the Linux system and some demo application, when I select Ethernet settings I see MAC address, and status UP but no IP addess and no more network parameters.

I´m trying to input the data but there are no console terminal to execute ipconfig command and no vi or text editor to set into /etc files.

My development is under RTOS but I want to verify that board is working with Linux.