This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320C6713B: out file not found

Part Number: TMS320C6713B


Tool/software: Code Composer Studio

Hi everyone, I got this error but I don't know what's wrong with my code. please help!

**** Build of configuration Debug for project try4 ****

"C:\\ti\\ccsv5\\utils\\bin\\gmake" -k all 

'Building target: try4.out'

'Invoking: C6000 Linker'

"C:/ti/ccsv5/tools/compiler/c6000_7.4.23/bin/cl6x" --abi=coffabi -g --display_error_number --diag_warning=225 --diag_wrap=off -z -m"try4.map" -i"C:/ti/ccsv5/tools/compiler/c6000_7.4.23/lib" -i"C:/ti/ccsv5/tools/compiler/c6000_7.4.23/include" --reread_libs --warn_sections --display_error_number --diag_wrap=off --xml_link_info="try4_linkInfo.xml" --rom_model -o "try4.out"  "./main.obj" "../C6713.cmd" -l"libc.a" 

<Linking>

warning #10210-D: creating ".stack" section with default size of 0x400; use the -stack option to change the default size

 undefined first referenced

  symbol       in file     

 --------- ----------------

 _length   ./main.obj      

error #10234-D: unresolved symbols remain

error #10010: errors encountered during linking; "try4.out" not built

>> Compilation failure

gmake: *** [try4.out] Error 1

gmake: Target `all' not remade because of errors.

**** Build Finished ****

Here is the code:

#include<stdio.h>

#include <math.h>

#include<signal.h>

void medianfilter(short* signal, int signalLength, short* output, int windowSize)

{

int i,j,k;

   //   Move window through all elements of the signal

for (i = 2; i < signalLength - 2; i++)

   {

      //   Pick up window elements

      float window[5];

      for (j = 0; j < 5; j++)

      { window[j] = signal[i - 2 + j];

      }

      //   Order elements (only half of them)

      for (j = 0; j < 3; j++)

      {

         //   Find position of minimum element

         int min = j;

         for (k = j + 1; k < 5; k++)

            { if (window[k] < window[min])

            min = k;

            }

         //   Put found minimum element in its place

         float temp = window[j];

         window[j] = window[min];

         window[min] = temp;

      }

      //   Get result - the middle element

      output[i - 2] = window[2];

   }

}

int main()

{

short inputSignal[102] = {0,2.8,3.24,5.374,5.2488,5.9049,6.3773,6.6962,7.8875,7.9736,6.9736,

7.9038,7.7783,6.6089,6.4055,6.1767,5.9297,6.6702,5.4034,6.1332,4.8631,4.5956,4.333,5.077,3.8288,

3.5895,3.3598,3.1401,2.9307,2.7319,2.5435,2.3654,2.1976,2.0396,1.8913,1.7522,1.622,1.5004,2.3868,

1.281,1.1825,1.0908,1.0057,0.92667,0.8534,0.78552,0.72268,0.66455,0.61082,0.56119,0.51538,0.47312,

0.43415,0.39825,0.36519,0.33476,1.3068,0.28101,0.25735,0.23561,0.21564,0.19731,0.18049,0.16506,0.15091,

1.1379,0.12606,0.11517,0.1052,0.096075,0.087721,0.080077,0.073084,0.066689,1.0608,0.055498,0.050614,0.046152,

0.042077,0.038354,0.034956,0.031854,0.029022,0.026438,1.0241,0.021931,0.01997,0.018182,0.016552,0.015066,

0.013712,0.012478,0.011353,0.010329,1.0094,0.0085466,

0.0077729,0.0070685,0.0064272,0.0058435,0.0053123,0.0048289};

int signalLength = length(inputSignal);

int windowSize3 =3; int windowSize5 = 5; int windowSize7 = 7;

short output3[102], output5[102], output7[102];

void medianfilter(short* inputSignal, int signalLength, short* output3, int windowSize3);

void medianfilter(short* inputSignal, int signalLength, short* output5, int windowSize5);

void medianfilter(short* inputSignal, int signalLength, short* output7, int windowSize7);

}