This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6472 Tracer Support

Hello,

 

Does the C6472 support Blackhawk tracer XDS560?

On the list of trace-enabled devices I see the C6486 (which is supposedly the same as the 72), but I don't see the 72 itself.

If it is, is there any document describing how to use the tracer with CCS4?

 

Thanks.

  • Where did you find "the list of trace-enabled devices"?

    On the XDS560 Trace Emulator or XDS560TRACE Product Folder, the list of trace-enabled devices does not include the C6472, but it may be a bit out-of-date. It does state that "The XDS560 Trace is designed for use with trace-enabled DSP processors", and the C6472 datasheet says it supports Trace and that it has the extra EMUnn pins that are needed, EMU18:2.

    Have you looked through the TI Wiki Pages for possible support comments?