This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI sd card flash utility Issue



I have been trying to make sd card flashable so that I can write to nand memory of DM365 .I have followed the steps given

by to make sd card bootable and flash nand memory of DM365.

But I was not able to format the sd card . It gives me following error.

sfdisk: ERROR: sector 0 does not have an msdos signature
 /dev/sdb: unrecognized partition table type

Old situation:
No partitions found
Warning: given size (150000) exceeds max allowable size (1020)

sfdisk: bad input
Failed to format SD card.

but when run following command parted -l /dev/sdb it gives me mdos parttiton .

The card I am using is of 8Gb.

I have found this issue in most of the cards. Only few card works with it . Is it card specific?

Please can anyone help me in resolving this issue.