Part Number: AM5728
Tool/software: Linux
I am developing a driver for exchanging data by using psnap(skb buff) modules.But I am getting the following crash. My kernel version is 4.9.41.
, *pmd=00000000[ 125.914637] Internal error: Oops: 206 [#4] PREEMPT SMP ARM [ 125.920145] Modules linked in: sample_gadget(O) libcomposite(O) psnap(O) llc(O) bc_example(O) sha512_generic sha512_arm sha256_generic sha1_generic sha1) [ 126.000132] CPU: 1 PID: 500 Comm: systemd-logind Tainted: G D O 4.9.41-ge3a80a1c5c #1 [ 126.008949] Hardware name: Generic DRA74X (Flattened Device Tree) [ 126.015064] task: ed210000 task.stack: ed31c000 [ 126.019621] PC is at __kmalloc_track_caller+0xa8/0x1d8 [ 126.019671] Unable to handle kernel paging request at virtual address 01092a85 [ 126.019675] pgd = d57867c0 [ 126.019681] [01092a85] *pgd=95795003, *pmd=00000000 [ 126.039624] LR is at get_mem_cgroup_from_mm+0xd4/0x12c [ 126.044781] pc : [<c03209fc>] lr : [<c0323414>] psr: 200f0013 [ 126.044781] sp : ed31dc78 ip : ed31dc30 fp : ed31dc9c [ 126.056303] r10: 00000000 r9 : 00001d1e r8 : ed31dc78 [ 126.061547] r7 : ed31c000 r6 : 01092a85 r5 : 025106c0 r4 : ee801c00 [ 126.068098] r3 : 00000000 r2 : 2deda000 r1 : 00001d1e r0 : ee801c00 [ 126.074650] Flags: nzCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment user [ 126.081812] Control: 30c5387d Table: ad24bd80 DAC: 55555555 [ 126.087578] Process systemd-logind (pid: 500, stack limit = 0xed31c210) [ 126.336637] Backtrace: [ 126.339103] [<c0320954>] (__kmalloc_track_caller) from [<c079e308>] (__kmalloc_reserve.constprop.15+0x2c/0x78) [ 126.349144] r9:0000000a r8:00000100 r7:c079fd74 r6:025004c0 r5:025004c0 r4:ed31dccf [ 126.356920] [<c079e2dc>] (__kmalloc_reserve.constprop.15) from [<c079fd74>] (__alloc_skb+0x60/0x144) [ 126.366088] r9:0000000a r8:00000000 r7:ee801cc0 r6:025004c0 r5:0000000a r4:ca4da240 [ 126.373864] [<c079fd14>] (__alloc_skb) from [<c079fea8>] (alloc_skb_with_frags+0x50/0x1d4) [ 126.382160] r9:0000000a r8:00000003 r7:c026e1f8 r6:00000000 r5:7fffffff r4:ee01de40 [ 126.389935] [<c079fe58>] (alloc_skb_with_frags) from [<c07968b8>] (sock_alloc_send_pskb+0x1f0/0x20c) [ 126.399104] r10:00000000 r9:0000000a r8:ee01df84 r7:c026e1f8 r6:ed31c000 r5:7fffffff [ 126.406960] r4:ee01de40 [ 126.409505] [<c07966c8>] (sock_alloc_send_pskb) from [<c084d8b8>] (unix_dgram_sendmsg+0x138/0x648) [ 126.418500] r10:00000016 r9:00000000 r8:0000000a r7:dff2b500 r6:ee01de40 r5:ed31df48 [ 126.426356] r4:00000000 [ 126.428901] [<c084d780>] (unix_dgram_sendmsg) from [<c07942ac>] (sock_sendmsg+0x1c/0x2c) [ 126.437023] r10:00004000 r9:00000000 r8:ed31de28 r7:dff2b500 r6:00000000 r5:00000000 [ 126.444880] r4:ed31df48 [ 126.447423] [<c0794290>] (sock_sendmsg) from [<c0794808>] (___sys_sendmsg+0x1d8/0x1e8) [ 126.455371] [<c0794630>] (___sys_sendmsg) from [<c079553c>] (__sys_sendmsg+0x48/0x74) [ 126.463231] r10:00000000 r9:ed31c000 r8:c0207d84 r7:00000128 r6:dff2b500 r5:00004000 [ 126.471089] r4:be80da10 [ 126.473630] [<c07954f4>] (__sys_sendmsg) from [<c0795578>] (SyS_sendmsg+0x10/0x14) [ 126.481227] r6:00000010 r5:be80dfa3 r4:be80da10 [ 126.485864] [<c0795568>] (SyS_sendmsg) from [<c0207be0>] (ret_fast_syscall+0x0/0x34)
This is my sample code I used for sending data,
int tx_data(void *buf, uint16_t len)
{
struct sk_buff *skb = NULL;
uint16_t hdr_len;
hdr_len = dll_dev->net_dev->hard_header_len + 8;
skb = alloc_skb(hdr_len + len, GFP_ATOMIC);
if (skb == NULL)
return -ENOMEM;
skb_reserve(skb, hdr_len);
skb_reset_transport_header(skb);
skb_reset_network_header(skb);
skb->dev = dll_dev->net_dev;
memcpy(skb->data, buf, len);
skb_put(skb, len);
dll_dev->proto->request(dll_dev->proto, skb, dll_dev->dmac);
return 0;
}
Usually The sk_buff is allocated by me on the send side through "alloc_skb" and given to the network. It's basically free'd by the network driver after send. But I am suspecting skb is not freeing by network driver. Is there a way to ensure the network driver is freeing skb properly.