Part Number: TMS320C6678
Dear Keystone Support Team,
My customer has the SPI BOOT problem using C6678.
Status;
-Hardware: C6678 Custom board
-Software: Based on MCSDK
-Boot error occured 2 units of 30 custome boards at normal tempareture
-Above 2 error units can boot on around 45℃
He has found that "iBootstatusLocl" was cleared at "setting Pcie_setMode" on the error units.
Then he has tried the following workaround.
(Original setting)
After BootComplete...
1. GPIO initialized
2. PCIE initialized
3. Other peripherals initialized
(Customer's workaround)
After BootComplete...
1. PCIE initialized
2. GPIO initialized
3. Other peripherals initialized
Question:
Is my customer's workaround a logcal step?
Is there any sequence for initialization for C6678?
Best regards,
Kanae