Part Number: AM3354
Background: Customer had been mass producing with AM3354 for ~ 1 year without issues.
During recent build, 14% of the units showed a USB1 VBUS failure to supply 5V. Swap tests performed and issue followed AM3354, not PCB or PMIC.
To help customer narrow down to the root cause, here are 2 main questions:
(i) what are the possible causes of USB1_DRVVBUS toggling at startup?
(ii) what could cause the VBUS to clamp at 3.3V when the supply +5V looks stable?
Image below shows the captures on 5V supply, USB1_VBUS & USB1_DRVVBUS.