Part Number: TMDSIDK437X
Other Parts Discussed in Thread: TMDXSK437X
Tool/software: Linux
I´m using the AM437x Starter Kit with TI Linux.
I configured network with ifconfig but it don´t communicate.
On ping command we can see ARP request with Wireshark but the TMDXSK437X don´t answer the ping.
I connected SK and PC with by a switch.
These are the logs :
ethtool
[ 1.855257] cpsw 4a100000.ethernet: Detected MACID = c4:be:84:cc:a6:9a
[ 1.870272] cpsw 4a100000.ethernet: cpsw: Detected MACID = c4:be:84:cc:a6:9c
[ 22.268315] net eth0: initializing cpsw version 1.15 (0)
[ 22.351775] net eth0: phy found : id is : 0x221622
[ 1652.003173] net eth1: initializing cpsw version 1.15 (0)
[ 1652.081839] net eth1: phy found : id is : 0x221622
boot log:
** Unable to read "uboot.env" from mmc0:1 **
Using default environment
Net: <ethaddr> not set. Validating first E-fuse MAC
cpsw, usb_ether
Hit any key to stop autoboot: 0
[ 1.804269] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6
[ 1.810392] davinci_mdio 4a101000.mdio: detected phy mask ffffffcf
[ 1.818277] platform sound: Driver asoc-simple-card requests probe deferral
[ 1.826769] libphy: 4a101000.mdio: probed
[ 1.830812] davinci_mdio 4a101000.mdio: phy[4]: device 4a101000.mdio:04, driver unknown
[ 1.838899] davinci_mdio 4a101000.mdio: phy[5]: device 4a101000.mdio:05, driver unknown
[ 1.855257] cpsw 4a100000.ethernet: Detected MACID = c4:be:84:cc:a6:9a
[ 1.862313] platform sound: Driver asoc-simple-card requests probe deferral
[ 1.870272] cpsw 4a100000.ethernet: cpsw: Detected MACID = c4:be:84:cc:a6:9c
[ 1.878753] platform sound: Driver asoc-simple-card requests probe deferral
[ 1.886488] omap_rtc 44e3e000.rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800)
ALSA: Restoring mixer settings...
Mon Jul 6 22:12:00 UTC 2015
INIT: Entering runlevel: 5
Configuring network interfaces... [ 22.268315] net eth0: initializing cpsw version 1.15 (0)
[ 22.351775] net eth0: phy found : id is : 0x221622
udhcpc (v1.22.1) started
Sending discover...
Sending discover...
Sending discover...
No lease, forking to background
done.
Starting