This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM1808 booting via NFS

Other Parts Discussed in Thread: AM3517

Hi All,

 

I'm working with an AM3517 EVM Development Kit.

I’m trying to boot via tftp and use nfs as root filesystem. Target gets ip by a dhcp server, and I see it is always 192.168.0.7.

 

On the Ubuntu server (192.168.0.31) I’ve put in /etc/exports the following line:

 

  /home/gabriele/workdir/filesys *(rw,sync,no_subtree_check)

 

Then, in /etc/hosts.allow:

 

  portmap mountd nfsd statd lockd rquotad : 192.168.0.7

 

while, in /etc/hosts.deny:

 

  portmap mountd nfsd statd lockd rquotad : ALL

 

Then I start services:

 

  host$ sudo service portmap start

  host$ sudo /etc/init.d/nfs-kernel-server restart

 

On the target side, after the uImage tftp transfer, I am getting the following error related to nfs

 

Sending DHCP requests .

PHY: 1:00 - Link is Up - 100/Full

., OK

IP-Config: Got DHCP answer from 0.0.0.0, my address is 192.168.0.7

IP-Config: Complete:

     device=eth0, addr=192.168.0.7, mask=255.255.255.0, gw=192.168.0.221,

     host=192.168.0.7, domain=intranet.cosmed.it, nis-domain=(none),

     bootserver=0.0.0.0, rootserver=192.168.0.31, rootpath=

Looking up port of RPC 100003/2 on 192.168.0.31

rpcbind: server 192.168.0.31 not responding, timed out

 

Don't know what am I missing on host.

Any help would be much appreciated.

 

Regards

Gabriele