Part Number: CCSTUDIO
Tool/software: Code Composer Studio
Hi there,
I need to use the USB (Full speed) with C5517.
I notice that on the EVM schematics DP and DM lines are directly connected from the DSP to the USB connector. The USB enumeration require a 1.5k pullup resistor for the speed recognition: how is it handled by the C5517? I couldn't find a register for the configuration of on-chip pullup resistor selection releted to USB_DP/USB_DM. Do I need to add an external pullup resistor or it is built-in on the C5517 chip?
Thank you