Hi, i confront with the same problem: Assertion failed, (0 != timeout), file Mcasp.c, line 3683 at the stdout window. The board woks alright last night. This message showed up once and disappeared after I reload the program. But when i retry it this morning, this error came out. It is the same with the original audioSample.pjt (for C6747). Nothing changed in hardware (OMAP-L137 EVM REV E) such as switch, etc. I hope it is not true that the AIC3106 become broken in one night.
Here is the software version that i use:
OMAP-L137 EVM REV E
CCS V3.3.81
BIOS 5.55.05
EDMA edma3_lld_01_07_00_01
pspdrivers_01_20_00_10
The following is erros screenshot:
Can anybody told me is there any other possibilities? Or I have to change another AIC3106?