Part Number: TMDXEVM8148
Other Parts Discussed in Thread: WL1271
Tool/software: Linux
Hello people,
We recently purchased the DM8148 EVM board - TMDXEVM8148 for our application development as this board was suiting our requirements. When going through the SDK and I would like to get few points clarified from TI :
1) The SDK provides Linux kernel 2.6.37 which is a very old version. It was surprising that TI hasn't migrated to some of the stable latest kernels. Is there any reason why TI hasn't provided the SDK with latest kernels?
2) Is it possible to migrate to some of the latest stable kernels ? If so any guidance/procedure is available from TI? Can you please support
3)The SDK has Angstrom Linux. We would like to migrate to minimal Ubuntu arm or some other latest distribution. Is this possible ? If so any guidance/procedure is available from TI?
4) We would also like to add a suitable WLAN USB mini adapted for WiFi feature onto this EVM board. Can TI Suggest any suitable/compatible chipset based adapter with procedure to build them. I have gone through the docs and wiki page of ti. They suggest the WL1271 based boards. But this board is not available in the market to purchase. Hence we would like to use the WLAN USB.
Kindly provide suggestions on this.