Tool/software: Linux
Hello Community,
I have a arm application which inits syslink and start the dsp application. They communicate over MessageQs between each other which works fine.
Then I have a second arm application which starts after this on the same arm processor. It calls also SysLink_setup and use a MessageQ to communicate with another task on the DSP.
When the second arm application wants to exit is stucks at syslink_destroy.
Tested Syslink Versions: 2_10_05_26 and 2_21_03_11
1. What's the reason for this behaviour?
2. Is it ok not to call syslink_destroy?
3. Is it allowed to use two arm applications on the same processor?
4. Does the second arm application needs its own MultiProc Id and must the dsp to use ipc_attach to this new id?
Best regards