Other Parts Discussed in Thread: AMIC120, AMIC110
Tool/software: TI-RTOS
Hi Team,
My customer decided to use the AMIC120 for the ProfiNET solution, as AM4377 shares the same design, so I marked this question with AM4377.
By checking the design of the AMIC110 ICE EVM. It was found that two 25MHz OSC are used for each ProfiNET port's PHY.
As the project is really cost-sensitive, they'd like to ask whether the two 25MHz OSC could be replaced by the clock output of the MPU? This could save the cost of the two OSCs.
If not, is it possbile to have the two ProfiNET port PHYs share the same 25MHz OSC, which can save them the cost of one OSC?