This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6742: OSCDIV register

Guru 10165 points
Part Number: TMS320C6742


 

Dear C6000 support team,

 

I have a question to the below Description in C674x TRM.

www.tij.co.jp/.../spruh81c.pdf

**********************************************************

Table 7-24. PLLC0 Oscillator Divider 1 Register (OSCDIV) Field Descriptions

OD1EN[bit15]

Value: 0

Description: Oscillator divider 1 is disabled.

**********************************************************

 

When does it set "0" to disable?

I would like to just make sure it.

 

Best regards,

Kanae