Other Parts Discussed in Thread: OMAP-L137
Hi,
A basic question about EMIFA.
If CS0 is used for SDRAM Memory, can CS4,CS5 still be used for other devices.
Thankyou in advance.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Prad,
The datasheet places a limitation on the maximum number of memory components you can share on the EMIFA bus without external signal buffers. Also, SDRAM requires regular memory refreshes so you will need to use an SDRAM that support self-refresh if asynch memory is to be used at the same time.
-Tommy
Hello Tommy,
I think SDRAM uses CAS and RAS pins, but these pins are multiplexed with CS4 and CS5,
In this case if SDRAM is used we cannot use CS4 and CS5?
Is this the limitation what you are saying?
and in our case we need to use SDRAM, FPGA or CPLD, Flash, Fram devices with EMIFA interface.
Please let me know what could be best way.
Thankyou,
Prad.