This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM3358: RTC accuracy

Part Number: AM3358


Tool/software: Linux

Hello ti community,

 

I want to use the internal rtc from the am3358 in a Linux System. In our application, we need a lot of time stamps for some data in a database. The application sync the System over an ntp request, but our system can’t request for every timestamp the ntp. My question is about the free running time and the accuracy from the internal rtc of the am3358. Is there any documentation about the accuracy from the rtc used with the internal 32 kHz clock over time and temperature?

 

thanks

Steven