Hi,
a customer is seeing output timing difference between datasheet & on board measurement.
He is willing to understand & clarify the cause of it.
- Input setup time (CMD): spec min/max : 6.8/17.8ns - measure 4.6ns
- Input Hold time (CMD) : spec min/max : 3/14ns - measure 16ns
- Input set-up time (Data0) : spec min/max : 6.8/17.8ns - measure 3.6ns
- Input Hold time (Data0) : spec min/max 3/14ns - measure 17ns
- Setup time MMC_DAT0 valid before MMC_CLK rising clock edge : Max 13.7ns - Measure 14.9
...
Setup is AM3352 connected to eMMC with read & write initiated from AM3352/Linux
Thanks
Nicolas