This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM4376: 128MB QSPI flash memory access

Part Number: AM4376
Other Parts Discussed in Thread: AM4378

Hi,

Our customers are using QSPI NOR flash memory with 128MB.
QSPI flash is accessed via memory mapped port. In this case, 64MB from 0x30000000 to 0x33FFFFFF can be accessed,
but 64MB above it can not be accessed.
Please tell me how to do to access.

Which of the following is possible?
① Can it be set so that the memory area of 0x04000000 to 0x07FFFFFF of the QSPI flash memory is mapped to the memory area of 0x30000000 to 0x33FFFFFF of AM4378?
② Is it be accessed via the configuration port?

Best Regards,
Shigehiro Tsuda