Tool/software: Linux
My company wish to develop GTK application in C++, after few modifications to gtk+3 recipe in arago I was able to build it and include in rootfs. However I have a problem with gtkmm library - the build brakes on cairomm-1.11.2 at linking stage:
MACHINE=am335x-evm bitbake cairomm
| /bin/grep: /mnt/Build_disk/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/am335x-evm/home/tcwg-buildslave/workspace/tcwg-make-release/label/docker-trusty-amd64-tcwg-build/target/arm-linux-gnueabihf/_build/builds/destdir/x86_64-unknown-linux-gnu/arm-linux-gnueabihf/lib/libstdc++.la: No such file or directory | sed: can't read /mnt/Build_disk/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/am335x-evm/home/tcwg-buildslave/workspace/tcwg-make-release/label/docker-trusty-amd64-tcwg-build/target/arm-linux-gnueabihf/_build/builds/destdir/x86_64-unknown-linux-gnu/arm-linux-gnueabihf/lib/libstdc++.la: No such file or directory | arm-linux-gnueabi-libtool: error: '/mnt/Build_disk/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/am335x-evm/home/tcwg-buildslave/workspace/tcwg-make-release/label/docker-trusty-amd64-tcwg-build/target/arm-linux-gnueabihf/_build/builds/destdir/x86_64-unknown-linux-gnu/arm-linux-gnueabihf/lib/libstdc++.la' is not a valid libtool archive | Makefile:510: recipe for target 'libcairomm-1.0.la' failed
It looks like the libpath is too long with unexpected home dir in the middle. I've tried also newer version cairomm-1.15.5 but it fails on configuration stage.
Did anybody included gtkmm and all its dependencies into arago?
These are the changes i had to make in gtk+3:
diff --git a/meta/recipes-gnome/gtk+/gtk+3.inc b/meta/recipes-gnome/gtk+/gtk+3.inc
index 83e9b92..f9962af 100644
--- a/meta/recipes-gnome/gtk+/gtk+3.inc
+++ b/meta/recipes-gnome/gtk+/gtk+3.inc
@@ -49,7 +49,7 @@ PACKAGECONFIG[x11] = "--enable-x11-backend,--disable-x11-backend,at-spi2-atk fon
# this is provided by oe-core patch that removes epoxy/gl dependency from a X11 build
PACKAGECONFIG[opengl] = "--enable-opengl,--disable-opengl,libepoxy"
PACKAGECONFIG[glx] = "--enable-glx,--disable-glx,,libgl"
-PACKAGECONFIG[wayland] = "--enable-wayland-backend,--disable-wayland-backend,wayland wayland-protocols libxkbcommon virtual/mesa wayland-native"
+PACKAGECONFIG[wayland] = "--enable-wayland-backend,--disable-wayland-backend,wayland wayland-protocols libxkbcommon wayland-native"
do_install_append() {
mv ${D}${bindir}/gtk-update-icon-cache ${D}${bindir}/gtk-update-icon-cache-3.0
@@ -100,7 +100,7 @@ GTKBASE_RRECOMMENDS ?= "liberation-fonts \
shared-mime-info \
adwaita-icon-theme-symbolic \
"
-GTKGLIBC_RRECOMMENDS ?= "${GTKBASE_RRECOMMENDS} glibc-gconv-iso8859-1"
+GTKGLIBC_RRECOMMENDS ?= "${GTKBASE_RRECOMMENDS} glibc"
RRECOMMENDS_${PN} = "${GTKBASE_RRECOMMENDS}"
RRECOMMENDS_${PN}_libc-glibc = "${GTKGLIBC_RRECOMMENDS}"
I know that i should do that in bbappend file, I'll clear everything out when it works.