Part Number: AM5728
Tool/software: Linux
Hi
I am following how to build SDK from this page
http://processors.wiki.ti.com/index.php/Processor_SDK_Building_The_SDK#Host_Setup
I followed all step down until this command
MACHINE=am57xx-evm bitbake arago-core-tisdk-image
The build stop by throwing this kind of Errors
ERROR: Function failed: do_compile (log file is located at /media/tctl/0d77dd17-3111-4b96-99e6-d85ff289d85a/tctl/Projects/TI_AM572XX/SDK_BUILD/tisdk/build/arago-tmp-external-linaro-toolchain/work/am57xx_evm-linux-gnueabi/pruss-lld-rtos/01.00.00.07-r0.0/temp/log.do_compile.19221)
ERROR: Task (/media/tctl/0d77dd17-3111-4b96-99e6-d85ff289d85a/tctl/Projects/TI_AM572XX/SDK_BUILD/tisdk/sources/meta-processor-sdk/recipes-bsp/pruss-lld/pruss-lld-rtos_git.bb:do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 3381 tasks of which 3369 didn't need to be rerun and 1 failed.
I have uploaded the error log herehttps://pastebin.com/4hptwZNi
Any suggestion would be appreciated.
Thank you
Aslam