Part Number: PROCESSOR-SDK-AM335X
Other Parts Discussed in Thread: TFP410
Tool/software: Linux
hi every one anyone can help?
i have succesfull to add splash screen in u-boot, but after that when i load the kernel it cannot boot, have error like this:
loading /boot/vmlinuz-3.14.55xeno ...
7364496 bytes read in 486 ms (14.5 MiB/s)
loading /boot/dtbs/3.14.55xeno/am335x-boneblack.dtb ...
86386 bytes read in 28 ms (2.9 MiB/s)
loading /boot/initrd.img-3.14.55xeno ...
3288421 bytes read in 226 ms (13.9 MiB/s)
debug: [console=ttyO0,115200n8 root=UUID=8887b14a-292b-471a-8239-d1bdbd3333ae ro rootfstype=ext4 rootwait coherent_pool=1M quiet cape_universal=enable] ...
debug: [bootz 0x82000000 0x88080000:322d65 0x88000000] ...
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Using Device Tree in place at 88000000, end 88018171
Starting kernel ...
[ 0.001139] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
[ 0.001147] This ensures that you still see kernel messages. Please
[ 0.001155] update your kernel commandline.
[ 2.736216] musb-hdrc musb-hdrc.0.auto: Failed to request rx1.
[ 2.742175] musb-hdrc musb-hdrc.0.auto: musb_init_controller failed with status -517
[ 2.816011] musb-hdrc musb-hdrc.1.auto: Failed to request rx1.
[ 2.821960] musb-hdrc musb-hdrc.1.auto: musb_init_controller failed with status -517
[ 2.961679] cpu cpu0: cpu0 clock notifier not ready, retry
[ 2.978283] Error: Driver 'tfp410' is already registered, aborting...