This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3354: Event queue entry register question

Guru 15520 points

Part Number: AM3354

Hi,

I have a question about AM335x EDMA.

In TRM(spruh73p) page.1678 Table 11-60 "Q0E0 Register Field Descriptions",
there are description of bit[7:6] ETYPE and written as follow:
***************************
0h = Event triggered via ER
1h = Auto-triggerd via QER
***************************

EDMA have 4 type of trigger events but there are only two of it.
Where are manually-trigger and chained trigger?
And it seem the value is uncorrect for Auto-trigger.

In the same page "11.4.1.35 Q0E0 Register", there following sentence:
*********************************************************************
For example, if the value in Q1E4 is read as 000 004Fh, this means the 4th entry in
queue 1 is a manually-triggered event on DMA channel 15.
*********************************************************************
In this example ETYPE value is 1h and it said it is manually-triggered.
What is the correct value for all type of event?

In other device's EDMA3, for example C6455, ETYPE value is as follow:
**********************************
0h = Event triggered via ER
1h = Manual triggered via ESR
2h = Chained triggered via CER
3h = Auto-triggered via QER
**********************************
Is this value same against AM335x EDMA3?

best regards,
g.f.