Hello,
Is there someone who already used the leds-omap-pwm.c ?
How do i have to configure this driver in the "/arch/arm/mach-omap2/board-var-om35xx.c"
on the OMAP3530 i see the driver under "/sys/bus/platform/drivers/leds_omap_pwm"
regards, Henk
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Is there someone who already used the leds-omap-pwm.c ?
How do i have to configure this driver in the "/arch/arm/mach-omap2/board-var-om35xx.c"
on the OMAP3530 i see the driver under "/sys/bus/platform/drivers/leds_omap_pwm"
regards, Henk
Michael,
I used the customboard from variscite for testing but at this moment we have developped our own board with the OMAP3530SBC v1.3 as controller
http://www.variscite.com/index.php?option=com_content&view=article&id=98&Itemid=63
I use the " VAR-OM35xxSBC and VAR-OM35xxLINUX SDK."
Linux version 2.6.29-rc3-omap1
I hope these are your answers.
Regards, Henk H
Henk:
The file you mentioned "/arch/arm/mach-omap2/board-var-om35xx.c" is not included in our OMAP3
Platform Support Package (which is specific to the TI evaluation boards). It must have been provided
by your hardware vendor. Please see if the hardware vendor can provide support. Have you
been able to resolve the issue?
Regards,
Michael T
PS: Please mark this post as answered via the Verify Answer button below if you think it answers your question. Thanks!