This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

virtual and physical address space

Hello I am Karthik,

I  am doing project in omap 3530 interfacing with ov5642 camera module. In that i am supposed to rotate the incoming video.

Here it is given two methods both in memory subsystem (virtual rotation frame buffer) and display subsystem (DMA).

 But it is given that VRFE is better than DMA.

In VRFE, i am confused  over virtual address space (0x7000 0000 - 0x7FFF FFFF, 0xE000 0000 - 0xFFFF FFFF) and physical address space (0x8000 0000 - 0xBFFF FFFF).

What is the purpose of virtual address space?

And one more question?

What will happen if i rotate the image 90 degrees. Will the image be cropped or the image get streched to the required screen size.

In spruf98g file it is not given clearly.

Please clarify my doubt.

 

With thanks and regards,

Karthik.