Part Number: AM3352
Tool/software: Linux
Hi All,
we made a customized board with AM3352 processor, 1GB DDR3 and 512 MB Nand flash. we are using am335x-evm-linux-rt-sdk-src-04.00.00.04.tar.xz and arago-base-tisdk-image-beagleboard.ubi. we compiled and flashed the Linux, filesystem and DTB in NAND Flash. We configured the console=ttyO2,115200n8.
When we give run nandboot, the following issue occur.
=> run nandboot
Booting from nand ...
NAND read: device 0 offset 0x80000, size 0x40000
262144 bytes read: OK
NAND read: device 0 offset 0x200000, size 0x800000
8388608 bytes read: OK
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8fff2000, end 8ffff75d ... OK
Starting kernel ...
We are using the
U-Boot version
VERSION = 2017
PATCHLEVEL = 01
Linux Version
VERSION = 4
PATCHLEVEL = 4
SUBLEVEL = 41
Filesystem
arago-base-tisdk-image-beagleboard.ubi
Regards,
Avinash N