Part Number: TMS320DM8148
Tool/software: Linux
DM8148 can work normally when set as an Endpoint with a x86 linux host.Howerver, x86_64 is more popular nowadays and will become the main host architecture in the coming future.
I got below err msg when operating DM8148 as Endpoint with Ubuntu 16.04 x86_64.
Does it need special configuration on the DM8148 side ? Can you help me with this problem or offer some demo ?
[ 4.729704] pcieport 0000:00:1c.0: AER: Multiple Corrected error received: id=00e0
[ 4.729711] pcieport 0000:00:1c.0: PCIe Bus Error: severity=Corrected, type=Physical Layer, id=00e0(Receiver ID)
[ 4.729714] pcieport 0000:00:1c.0: device [8086:9d15] error status/mask=00000001/00002000
[ 4.729717] pcieport 0000:00:1c.0: [ 0] Receiver Error (First)
[ 4.729720] pcieport 0000:00:1c.0: AER: Multiple Corrected error received: id=00e0
[ 4.729723] pcieport 0000:00:1c.0: can't find device of ID00e0
[ 4.729724] pcieport 0000:00:1c.0: AER: Multiple Corrected error received: id=00e0