This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320C6713B: EXTERNAL FLASH PROGRAMMING

Part Number: TMS320C6713B

Tool/software: Code Composer Studio

Good morning,

I'm using the TMS320C6713GDPA200 DSP on a card and this DSP is connected to its program FLASH on CS1
I would like to program thIs FLASH, mounted on the board and without a socket.

I have available:
Spectrum Digital XDS510PP PLUS emulator
CCS 3.1.0
Windows XP
FLASH: 4Mx16 TSOP48 MBM29DL640E-90 

I have access to pins: EMU0, EMU1, TMS, TRST, TDO, TDI, TCK.
Can I program the FLASH with the emulator without using an ATE or a JTAG program?

Best Regards