This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/PROCESSOR-SDK-AM335X: NIMU Basic Example issue

Part Number: PROCESSOR-SDK-AM335X


Tool/software: TI-RTOS

Hi,

I use the example project:NIMU_BasicExample_skAM335x_armExampleproject.
Modified the correct pin in skAM335x_pinmux.c,but is not work. I can't ping my board。
And the Network standard recognition error,print:"Negotiated connection: FullDuplex 1000 Mbs",but my network is "Negotiated connection: FullDuplex 100 Mbs"

The all Uart_print is:"

SetPhyMode:000021e1 Auto:1, FD10:64, HD10:32, FD100:256, HD100:128, FD1000:8192 LPBK:0
SetPhyMode:000021e1 Auto:1, FD10:64, HD10:32, FD100:256, HD100:128, FD1000:8192 LPBK:0
ENETPHY_FindingState: PhyNum: 0
ENETPHY_FindingState: PhyNum: 1
ENETPHY_DisablePhy(0)
Enable Phy to negotiate external connection
NWAY Advertising: FullDuplex-1000 FullDuplex-100 HalfDuplex-100 FullDuplex-10 HalfDuplex-10
ENETPHY_DisablePhy(1)
Enable Phy to negotiate external connection
NWAY Advertising: FullDuplex-1000 FullDuplex-100 HalfDuplex-100 FullDuplex-10 HalfDuplex-10
Negotiated connection: FullDuplex 1000 Mbs

"

ccs print:"Network Added: If-1:10.169.32.249"
the ip is correct
.