I have checked the documentation (SPRUF09) and it states only DMA Controller 3 has access to external memory. The examples I have looked at use channels 0-15. Are the channels mapped like this DMA Controller 0 (Channels 0-3), DMA Controller 1 (Channels 4-7), DMA Controller 2 (8-11), DMA Controller 3 (12-15)? Or do I need to set some specific attributes to use DMA Controller 3?
Also are there more examples I can look at?
Thanks in advance
Tommy