Other Parts Discussed in Thread: CDCE906
Hi
I have set the SW2 1-4 = 0011 and have tried
1) the fastboot SW3-3 equal to 0 and get nothing on hyperterm,
2) SW3-3 = 1 and get 'via output on hyperterm.
I have verified that the serial port to hyperterm link works by running the DVDSK uart example.
My switch settings are:
SW2 00111 01000 (should be no hardware flow control)
also tried
SW2 11001 01000 (should be no hardware flow control)
123..... .......10
SW3 11X10 10000
I have hyperterm set to 115600 baud.
Any ideas? Thanks in advance.
Note that the "Using the DM648 bootloader" doc spraa1jd.pdf says that the bootmode is 1000 for uart. But the rest of the ducment says 0011. I tried 1000 and it didn't work either.
1.10.1 UART Boot Timing
1.11 Ethernet Boot Modes - SGMII0 Only, SGMII0, and SGMII1 (Bootmode[3:0] = 1000b,
Boot-Mode Description www.ti.com
Operationally, UART boot via BOOTMODES[3:0] == 1000b and 1110b are essentially the same. The difference is management of data flow.