Part Number: TMS320C6713B
Tool/software: Code Composer Studio
I am able to build the model I want without any errors but some warnings. I am able to successfully debug as well. After I load the .out file I see this error on the console below which says "ISR overrun - base sample time is too fast" How do I overcome this? I am seeing this error even when I just load the .out file. Attached is the screenshot of that. It would of great help if someone can help me with this. I am also not able to listen to listen to any audio when I give the input. I am working on C6713 DSK using CCS5.3 and Matlab 2016a. This is the case with two other models as well.
Thank you
Akshay.